Novanta Global
Novanta Global
Novanta Česká republika s.r.o.
Londýnské náměstí 886/4
639 00 Brno – Štýřice
Czech Republic
Tel: +420 530 511 900
ID: 04851749
VAT: CZ04851749
The company is registered in the Commercial Register held by the regional court in Brno, Section C, File 94322.
Tel: +420 530 511 932
Email: customercare-EMEA@ndssi.com
Novanta Czech Republic is located in the Brno Business Park, Londýnské náměstí. The entire site, consisting of four administrative buildings, covers an area of 48,000 square meters and is located in the south of the city, directly opposite the Central Cemetery. Our R&D center and shared services are located in Building D and the service center is located in Building B.
The premises are optimally connected, not least thanks to the proximity to the D1 (E50) motorway and several public transport stops. From the airport, it is only about 15 minutes by car. The central train station is also accessible by tram in about 15 minutes, Mendlovo náměstí in eight minutes. Another advantage of the business park are the good parking facilities – in-house, in front of the building, or in the general area.
There are three restaurants on the grounds of the Business Park where you can have breakfast and lunch.